Вы находитесь на глобальной странице. Пожалуйста, выберите ваш рынок или регион, чтобы просмотреть содержимое для вашего местоположения и совершать покупки онлайн.
Vortex flowmeters are commonly designed as flanged or wafer types and typically have no moving parts, which reduces wear and maintenance needs.
There are different types of sensors, including capacitive, piezo-resistive, ultrasonic, thermistor, mechanical, pressure and strain-gauge sensors.
DSC sensors, used by Endress+Hauser, are robust and resistant to temperature shocks, water hammer, and pipe vibrations, while maintaininig accuracy.
СодержаниеСодержание
How are vortex flowmeters designed?
Vortex flowmeters consist of various components, including measuring tube, bluff body, sensor, preamplifier and meter electronics (see Fig. 1). In the majority of meters on the market, the sensors have no moving parts and, therefore, are not subject to wear and require no maintenance.
The two most common vortex meter body designs are those with flanges and those without. The latter is known as the wafer type and is designed for installation between two pipe flanges. Some wafer designs have a standardized overall length of 65 mm (2.5") which allows them to directly replace orifice assemblies.
The standard range available on the market covers nominal diameters from DN 15 to 300 (1/2 to 12"), with some versions up to DN 400 (16"). Pressure ratings can be up to PN 250 (ANSI Class 1500). The vortex frequencies of nominal diameters larger than DN 300 (12") are very low, and powerful signal processing is required in order to obtain a stable signal. For large diameter applications, vortex meters are relatively expensive in comparison to orifice plates. Many manufacturers also offer designs for very low or very high temperatures (–200 to +450 °C / –330 to +842 °F).
Devices with two independent sensors and electronics constitute a special case (Fig. 1). This design is primarily used in industries where redundancy measurement is considered important.
Fig. 1: Prowirl vortex flowmeters from Endress+Hauser (two-wire device). Left: Flange version, Middle: Wafer version, Right: Dualsens version with two sensors and electronics
How do vortex sensors work?
The vortices produced by the bluff body create local pressure fluctuations in the flow which can be measured by a variety of sensors and converted into electric signals. The types of sensors favored by individual manufacturers vary widely and include capacitive, piezo-resistive, ultrasonic, thermistor, mechanical, pressure and strain-gauge sensors. In most instances, the sensor is either integrated into the bluff body or situated immediately behind it. Most sensors today measure the vortex shedding capacitively or piezo-electrically.
The DSC sensors used by Endress+Hauser have a paddle-shaped sensor protruding behind the bluff body (Fig. 2). This paddle (a) transmits the vortex pressure fluctuations to a sleeve-like center electrode (c) that forms capacitors C1 and C2 together with the outside electrode (d), which consists of two half-shells. The change in the width of the gap produces a periodically varying change in capacitance that is proportional to the vortex pressure differential, which is processed by the meter electronics. The mechanical balancing of the sensor makes such measuring systems largely unaffected by pipeline vibrations.
Fig. 2: Design of a DSC sensor from Endress+Hauser. a = Sensor paddle, b = Focal point of the sensor system, c = Center electrode, d = Outer electrode
The primary advantages of the DSC sensor are:
Resistant to temperature shocks, for example in cryogenic applications (see Fig. 3) or in steam systems. The stainless steel DSC sensor has no moving parts or very sensitive components and is extremely robust.
Resistant to water hammer, e.g. in steam systems.
Unaffected by pipe vibrations. The distance between the center electrode and the outside electrodes is not influenced by the acceleration effects caused by vibrations. Sensor paddle and center electrode are exactly balanced, so the acceleration forces produced by vibrations always act at the sensor system’s center of gravity and, consequently, do not generate additional, vibration-related signals.
Largely unaffected by foreign matter, because the DSC sensor is mounted freely in the measuring tube. In worst-case conditions, deposits on the sensor paddle itself can produce a marginal reduction in measuring range (turndown), but do not influence the accuracy of (the) measurement.
At the end of the course you will know about the features of the PROFINET technology and the PA profiles, network design of 100BaseTX and Ethernet-APL.
Хотите принять участие в одном из наших мероприятий? Выберите по категории или отрасли.
Ваша конфиденциальность очень важна для нас
Мы используем файлы cookie для повышения удобства просмотра веб-страниц, сбора статистических данных для оптимизации функциональности сайта, а также для показа рекламы и контента, адаптированных специально под вас.
Выбирая опцию "Принять все", вы соглашаетесь с использованием нами файлов cookie.
Для получения более подробной информации ознакомьтесь с нашей Политикой использования файлов cookie .